Programs

A program contains the functions, function blocks, and the associated definitions in devices. A project can contain up to 256 programs.
Create programs using the following programming languages:
In
Project Organizer,
use the
Programs
node to:
  • Create controller programs.
  • Import a program from your computer to
    FactoryTalk Design Workbench
    .
  • Paste a copied program under the node to duplicate the program.
  • Add interrupts to the controller project.
  • Change the program execution order by moving the program before or after other programs.
  • Open a program.
  • Rename programs. Renaming a user program automatically updates all references to the program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal