Ladder diagram language

A ladder diagram (LD) is a graphical representation of Boolean equations that combines contacts (input arguments) with coils (output results).
The LD language uses graphic symbols in a program chart that is organized like a relay ladder wiring diagram to describe the tests and modifications of Boolean data.
LD graphic symbols are organized within the chart as an electrical contact diagram. The term "ladder" comes from the concept of rungs connected to vertical power rails at both ends, where each rung represents an individual circuit.
FactoryTalk Design Workbench
includes an LD language editor and supports specific elements and instructions that are provided exclusively by the
FactoryTalk Design Workbench
software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal