Work in the ladder diagram language editor

Elements are added to the ladder diagram language editor according to the following rules:
  • The first element on a rung is added at the position that you selected.
  • Subsequent elements are added to the right of the selected element on the rung.
  • It is not supported to insert an element to the right of a coil return or jump.
The methods to add elements to the LD program are as follows:
Methods to add an element to the LD program
Method
Description
Ladder editor
Adds, deletes, or copies and pastes elements.
Toolbox
Adds elements and instructions to the LD program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal