Duplicate a Program Organization Unit

In
Project Organizer
, copy and paste a Program Organization Unit (POU) to duplicate it in the same or between different FactoryTalk Design Workbench sessions, especially when you have similar POUs. The pasted POU will have a number appended to it if a POU with the same name exists.
TIP:
  • The pasting action pastes the latest version of the copied POU. Once a copied POU is pasted, any further edits won't update the pasted POU.
  • It is not supported to copy a program to a user-defined function block (UDFB).
  • It is not supported to paste a copied POU after it has been deleted.
Prerequisites
  • The controller is offline.
To duplicate a POU
  1. In
    Project Organizer
    , right-click the POU, and then select
    Copy
    .
  2. Right-click the node under which you want to paste the POU, and then select
    Paste
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal