Verify a Program Organization Unit

Use the
Verify program
context menu to verify the logic of a single Program Organization Unit (POU) without building the whole solution. The verification result shows on the
Output
pane. On
Project Organizer
, a symbol will display next to the POU name to indicate any errors or warnings.
To verify a POU
  • In
    Project Organizer
    , right-click the POU, and then select
    Verify program
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal