User-defined function blocks

Use the
User-Defined Function Blocks
node in Project Organizer to create logic programs for the
Micro800
controller in the following languages:
  • Function block diagram (FBD)
  • Ladder diagram (LD)
  • Structured text (ST)
User-defined function blocks (UDFBs) define business logic for complex mathematical computations. Once created, it can be reused like other function blocks in
FactoryTalk Design Workbench
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal