Project Organizer

Project Organizer
displays the devices and program elements of the project in an organized tree view. Use
Project Organizer
to open additional device configuration workspaces and manage program elements. If no device is added, use the New device or Discover Device button to add one. Elements displayed in
Project Organizer
vary with the added device.
For projects that contain a
Micro800
controller,
Project Organizer
displays the following items that are associated with the controller:
  • Global variables
  • Assets, including user-defined functions, user-defined function blocks, and user-defined data types
  • I/O configurations
Project Organizer
Project Organizer
Icons in Project Organizer
Item
Description
Add device button
Opens
Add device
to add devices to the project.
Delete device button
Deletes the selected device from the project.
Discover device button
Opens
Select Device
to view a list of devices that are connected to the computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal