Commands in Project Organizer

Use
Project Organizer
to open and edit additional device configuration options.
Micro800
controllers and drives are available in
Project Organizer
.

Commands available for Micro800 controllers

Commands available by right-clicking the Micro800 controller in Project Organizer
Right-click and select
To
Build
Connect
Disconnect
Download
Upload
Clean
Fault
Open
<controller-name>:Fault
to view and clear controller faults.
Diagnose
Secure
Change Controller
Import > Global variables
Import > Data types
Export > Global variables
Export > Data types
Delete
Remove the
Micro800
controller from
Project Organizer
. You can also use the
Delete
key.
Data protection
Open Data protection to add or remove variables from a list of the protected variables.
Memory module backup and restore
Open
Memory module backup and restore
to configure the relevant settings and start the backup or restore process.

Commands available for Class 1 devices, plug-in modules, and expansion modules

Commands available by right-clicking a Class 1 device, plug-in module, or expansion module in Project Organizer
Right-click and select
To
Delete
Remove a drive, plug-in module, or expansion module from
Project Organizer
. You can also use the
Delete
key to remove the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal