Upload a controller configuration from a controller

Use
Upload device
to upload a project containing programs, variables, and controller configurations from a
Micro800
controller to
FactoryTalk Design Workbench
. All project programs, variables, and controller configurations are overwritten after an upload. Once the project is uploaded to
FactoryTalk Design Workbench
, you can edit the controller project, and then download it back to the controller.
Prerequisites
  • Set the connection path for the controller.
  • The catalog number of the controller in the current project matches the one you're uploading from.
To upload a controller configuration from a controller
  1. Select Online center button to open
    Online center
    .
  2. In
    Online center
    , from the
    Device
    list, select the controller, and then select
    Upload
    .
  3. In
    Upload device
    , select
    OK
    .
    TIP: COP instruction blocks do not upload values for Src and Dest variables. Other instruction blocks and variables are not affected.
  4. Use the
    Output
    pane to view the result.
  5. If there are errors, resolve them, and then upload again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal