Secure a controller with a password

To prevent unauthorized access to the configuration and programming in a controller, it is recommended that you secure the controller with a password.
When a controller is configured with a password, you must enter the password before doing any of the following:
IMPORTANT:
If the existing password is forgotten or lost, it cannot be recovered, changed, or cleared. If a controller fault occurs during password configuration, restart the controller and reconfigure the password.
Prerequisites
  • The controller is in
    Remote program
    mode.
To secure a controller with a password
  1. Open
    Change password for <controller-name>
    by doing one of the following:
    • In
      Connection
      , select
      Secure
      , and then select
      Set password
      .
    • In
      Project Organizer
      , right-click the controller, and then select
      Secure
      Set Password
      .
    • In
      Project Organizer
      , select the controller, and then from the menu bar, select
      Device
      Secure
      .
  2. In
    Change password for <project-name>
    , enter a password. Passwords must be 8 to 64 characters long, which can include letters, numbers, spaces, and any keyboard symbols.
  3. In
    Confirmation
    , enter the exact password again.
  4. (optional) To view the password, select .
  5. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal