Change the controller password

Before changing the controller password, you must have the current password.
IMPORTANT:
If the existing password is forgotten or lost, there is no way to recover or change the password.
We recommend changing the controller password periodically to protect the programs and functions in the controller.
Passwords must be 8 to 64 characters long, which can include letters, numbers, spaces, and any keyboard symbols.
Prerequisites
  • The controller is in
    Remote program
    mode.
To change the controller password
  1. Open
    Change password for <controller-name>
    by doing one of the following:
    • In
      Connection
      , select
      Secure
      , and then select
      Change password
      .
    • In
      Project Organizer
      , right-click the controller, and then select
      Secure
      Change Password
      .
    • In
      Project Organizer
      , select the controller, and then from the menu bar, select
      Device
      Secure
      Change password
      .
  2. In
    Change password for <controller-name>
    , do the following:
    1. Enter your current password.
    2. Enter your new password.
    3. Enter your new password again to confirm it.
    To view the password, select View-password icon.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal