Clear the controller password

Before clearing the password for a
Micro800
controller, you must have the current password.
Prerequisites
  • The controller is in
    Remote program
    mode.
To clear the controller password
  1. Open
    Clear password for <controller-name>
    by doing one of the following:
    • In
      Connection
      , select
      Secure
      , and then select
      Clear password
      .
    • In
      Project Organizer
      , right-click the controller node, and then select
      Secure
      Clear Password
      .
    • In
      Project Organizer
      , select the controller, and then from the menu bar, select
      Device
      Secure
      Clear password
      .
  2. In
    Clear password for <controller-name>
    , enter the password.
    To view the password, select View-password icon.
  3. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal