Add a controller to the project

Use
Add device
to add a controller to a
FactoryTalk Design Workbench
project.
FactoryTalk Design Workbench
supports one controller for each project.
After selecting a controller, in the
Selection
pane of the
Add device
dialog, the following controller information is shown:
For more information about devices, see Controllers catalog.
Prerequisites
  • Create a project without adding a controller.
To add a device to a project
  1. Open
    Add device
    by doing one of the following:
    • In
      Project Organizer
      , right-click a blank space, and then select
      New device
      .
    • In
      Project Organizer
      , select the
      New device
      button.
  2. In
    Add device
    , double-click the controller you want to add or select the checkbox beside the controller.
  3. In
    Selection
    , enter the controller name, select the controller revision, view the controller lifecycle information, and then select
    Add
    .
    After adding a controller, it is recommended that you secure the controller with a password. Be sure to record and store the password securely, because it cannot be recovered if lost.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal