User interface

Use the
FactoryTalk Design Workbench
user interface (UI) to create projects, specify which panes to view, and reset to the default layout if necessary.
FactoryTalk Design Workbench user interface

          FactoryTalk Design Workbench user interface
Items on the UI
Item
Name
Description
callout_orange1
Contains the menu items for
FactoryTalk Design Workbench
and the active window.
callout_orange2
Toolbar
Contains:
  • The
    Save
    and
    Online center
    buttons.
  • The run mode change (RMC) toolbar with buttons to start online editing, test, accept, and finalize changes during RMC.
    If RMC changes are ongoing, not tested, or not accepted in a Program Organization Unit (POU), the following icons appear beside that POU in
    Project Organizer
    to indicate the changes:
    • resume RMC editing indicates that there are ongoing or unsaved RMC changes. Before reconnecting to the controller, you can choose to resume editing.
    • resume RMC testing indicates that testing is in progress on a POU. Before reconnecting to the controller, you can choose to continue testing the POU.
callout_orange3
Displays the devices, I/O configurations, and program elements of the project in an organized tree view.
callout_orange4
Contains the button toggles you use to show or hide specific panes.
callout_orange5
Contains:
  • A
    Console
    page that displays the added devices, their connection status, and log entries.
  • An
    Error list
    page that displays the descriptions, locations, and time stamps of errors, warnings, and messages.
  • A
    Log
    page that displays the log descriptions and time stamps.
callout1
Workspace
Contains the options to configure devices and build programs. The content varies with the page you open.
callout2
Connection pane
For each added device, the
Connection
pane contains:
  • The device name and catalog number.
  • The connection path to connect to the device if any.
  • The toggle to connect to or disconnect from the device.
  • The
    Controller mode
    list to view and change the controller connection mode.
  • The
    Fault
    button to open the
    Micro800
    controller's fault diagnostics page.
  • The
    Secure
    button to open the pages to set, clear, or change the controller password.
callout3
Contains the logic elements and instructions that can be added to the opened language editor.
callout4
Displays the properties of a selected item.
You can edit the properties in the
Properties
pane.
callout5
Error indicator
Displays the total number of errors in the current project, counting only errors from POUs that are built and verified.
callout6
Warning indicator
Displays the total number of warnings in the current project, counting only errors from POUs that are built and verified.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal