Online center

The
Online center
contains information on the added devices and the options to control the devices and configure the online settings:
  • The name, catalog number, and connection path of the added devices.
  • The
    Download
    and
    Upload
    button.
  • The messages about the download and upload progress.
  • A link to the Online settings page.
Use the
Online center
to:
  • Download device configurations.
  • Upload device configurations.
  • View the download and upload progress.
  • Change the device connection path.
  • Open
    Online settings
    to view and change the online settings.
Online center
Online center with callouts
Items in the Online center
Item
Description
callout1
Shows how many devices are selected in
Online center
.
callout2
Opens the Online settings page to configure relevant settings.
callout3
Indicates the device connection status.
  • Gray: The device is offline.
  • Green: The device is online.
  • Red: The device is offline and has faults.
callout4
Opens the
Select device
dialog to select a device to connect to.
callout5
Opens the
Download device
dialog to download the selected device configurations to the device.
callout6
Opens the
Upload device
dialog to upload the selected device configurations to
FactoryTalk Design Workbench
for editing.
callout7
Lists the added devices with the device names and catalog numbers.
callout8
Displays the device connection paths.
To change the connection path, do one of the following:
  • Double-click the
    Path
    box, and then enter the path.
  • Select Select device button, and then in
    Select device
    , enter a path.
callout9
Displays the status and time stamps of the actions that are performed on the added devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal