Online settings

Use the
Online settings
dialog to configure the controller's settings for communication, downloading, uploading, and device discovery.
Controller online settings
Category
Setting
Description
General
Use Cellular Network
Determines whether to use the cellular network for downloading and uploading.
The default setting is
No
.
Download
Mode
Sets the controller mode when downloading is completed.
The default setting is
Remote program
.
Connection
Determines whether to connect to the controller when downloading is completed.
The default setting is
Connect
.
Project value
Determines whether to download the values of the variables.
The default setting is
No
.
Warning
Determines whether to download the controller project that contains build errors.
The default setting is
Yes
.
Communication
Determines whether to download the project when the driver settings for Ethernet, USB, or DF1 differ in the controller and the project.
The controller cannot automatically establish a connection if you download mismatched configurations between the controller and the project.
The default setting for
Download Ethernet
is
No
.
The setting is applicable when using the same driver to download the corresponding driver settings for Ethernet, USB, or DF1.
The default setting for
Download Ethernet
,
Download USB
, or
Download Serial Port
is
No
.
Upload
Connection
Determines whether to connect to the controller when uploading is completed.
The default setting is
Connect
.
Project value
Determines whether to upload the values of variables.
The default setting is
No
.
Discover
Discover
Determines whether to connect to the controller and initiate debugging when discovery is completed.
The default setting is
Connect
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal