Toolbox

Use
Toolbox
to find and add program elements to a language editor.
Toolbox
contains the elements associated with the ladder diagram language, function block diagram language, or structured text language.
In
Toolbox
:
  • Use
    Search
    or select a category from the list to filter program elements.
  • Hover over an element to view its name, description, and image.
  • Drag the border between the category and list pane to resize the panes.
Working in Toolbox
To
Do this
Pin or unpin
Toolbox
Do one of the following:
  • Select pin button or unpin button .
  • Select pin or unpin button, and then select
    Pin
    or
    Unpin
    .
Shrink down
Toolbox
and leave just a tab
Select pin or unpin button, and then select
Collapse
.
Show the content of
Toolbox
Select pin or unpin button, and then select
Expand
.
Hide
Toolbox
Select pin or unpin button, and then select
Close
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal