Structured text Toolbox

Use the structured text (ST)
Toolbox
to add program elements to the ST diagram.
Toolbox
is displayed by default. If it is hidden, do one of the following:
  • From the pane bar, select Toolbox button.
  • From the
    View
    menu, select
    Toolbox
    .
ST Toolbox
ST Toolbox
ST editor Toolbox
Item
Description
Callout 1
Adds the code snippet IF-THEN-ELSEIF-ELSE-END_IF statement to the editor.
Callout 2
Adds the code snippet Case statement to the editor.
Callout 3
Adds the code snippet FOR statement to the editor.
Callout 4
Adds the code snippet WHILE statement to the editor.
Callout 5
Adds the code snippet REPEAT statement to the editor.
Orange callout 1
Displays the categories of the program elements. Selecting a category filters the displayed program elements.
Orange callout 2
Displays the program elements of the selected category.
Callout 6
Contains the entered element name for quick finding.
As you enter, elements that contain the search text appear in
Toolbox
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal