Function block diagram Toolbox

Use the function block diagram (FBD)
Toolbox
to add program elements to the FBD program.
Toolbox
is displayed by default. If it is hidden, do one of the following:
  • From the pane bar, select Toolbox toggle.
  • From the
    View
    menu, select
    Toolbox
    .
FBD Toolbox
FBD Toolbox
Function block diagram Toolbox
Item
Description
callout1
Creates a reference to an input variable.
callout2
Contains the entered element name for quick finding.
As you enter, elements that contain the search text appear in
Toolbox
.
callout3
Create a reference to an output variable.
callout4
Creates a reference to an input or output variable.
callout5
Contains the entered FBD program description. Descriptions are free-format text used for documentation purposes only and are not acted upon by the program.
callout_orange1
Displays the categories of the program elements. Selecting a category filters the displayed program elements.
callout_orange2
Displays the program elements of the selected category.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal