Language editors

Use the language editor to develop the content of Micro800 programs.
A language editor holds elements from the following programming languages:
  • Ladder diagram (LD)
  • Structured text (ST)
  • Function block (FB)
There is an additional language editor for user-defined function blocks (UDFBs).
In language editors:
  • Each program in a project opens a separate language editor in the application workspace, with program names shown on the workspace tab.
  • You can open several workspaces at the same time.
  • Use
    Toolbox
    to inset elements to the language editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal