Open the diagnostics pages
Use the
Device
menu, the Connection
pane, or one of the controller configuration pages to open the controller diagnostics pages.Prerequisites
- The controller is online.
To open the diagnostics pages
- Do one of the following:
- InConnection, select
to expand the controller information, and then select Diagnose. - InProject Organizer, select the controller, and then from theDevicemenu, selectDiagnose.
- From one of the following pages, selectDiagnose:
- Startup(Micro810LC10 controllers)
- Startup/Faults
- Serial Port
- Ethernet
- Memory Card
- LCD Module(Micro810LC10 controllers)
- Plug-in Modules - 2080-SERIALISOL
- Plug-in Modules - 2080-MEMBAK-RTC2
- Plug-in Modules - 2080-DNET20
Provide Feedback