Properties pane

Use the
Properties
pane to view and edit the properties of items in
Project Organizer
or language editors. Properties that appear dimmed are read-only.
The content that displays in the
Properties
pane varies with the item that you selected.
Items in the Properties pane
Selected Item
Content displayed in Properties
Controller
  • Controller name
  • Controller catalog number
Program Organization Unit (POU)
  • POU name
  • POU description
Instruction
  • Instruction name
  • Instruction description
  • EN/ENO
  • Input Number of the input operands for the selected instructions, such as the ADD instruction
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal