Controller application workspace
The controller application workspace is the main area where you view, configure, monitor, and troubleshoot
Micro800
controllers in a FactoryTalk Design Workbench
project.The controller application workspace contains the
Controller
tree and controller configuration pages.Controller tree and the General configuration page of an Micro870 L70E
controller

Controller tree
The
Controller
tree lists the available configurations for a Micro800
controller.The nodes in the
Controller
tree vary with the controller type. The following table lists the nodes in the Controller
tree.Node | Available for |
|---|---|
General | All |
Memory | All |
Startup/Fault | All |
Serial Port | Micro820 L20E, Micro850 L50E, and Micro870 L70E controllers |
USB Port | Micro820 L20E, Micro850 L50E, and Micro870 L70E controllers |
Ethernet | Micro820 L20E, Micro850 L50E, and Micro870 L70E controllers |
Modbus Mapping | Micro820 L20E, Micro850 L50E, and Micro870 L70E controllers |
MicroLogix Mapping | Micro850 L50E and Micro870 L70E
controllers |
Real Time Clock | All |
Motion | 2080-L50E- xx QBB, 2080-L50E-xx QVB, and 2080-L70E-xx QBB(N) controllers |
Remote LCD | Micro820 L20E, Micro850 L50E, and Micro870 L70E controllers |
LCD Module | Micro810 LC10 controllers |
Data Log | Micro820 L20E, Micro850 L50E, and Micro870 L70E controllers
|
Recipe | Micro820 L20E, Micro850 L50E, and Micro870 L70E controllersThe Manage recipe function is available when an SD card is added to the controller. |
Controller configuration page
The content on the controller configuration pages varies with the controller type and the tree node that you selected. Use the controller configuration page to:
- View and configure the relevant settings of the current controller.
- Resize the page.
Provide Feedback