Keyboard shortcuts

The following table introduces the keyboard shortcuts that apply universally.
Keyboard shortcuts
Name
Keyboard Shortcut
Description
Select all
Ctrl+A
Selects all elements on the current page.
Show/hide bottom panes
Ctrl+Shift+B
Displays or hides the panes that are last pinned at the bottom of the user interface (UI).
Copy
Ctrl+C
Copies the selected element to the clipboard.
Show/hide pane
Ctrl+Shift+C
Displays or hides the selected pane.
Find references
Ctrl+E
Finds all references to the selected variable.
Select variable
Ctrl+L
Opens
Select variable
from the ladder diagram (LD), function block diagram (FBD), or structured text (ST) editor to select a variable for the selected operand.
Show/hide left panes
Ctrl+Shift+L
Displays or hides the panes that are last pinned to the left side of the UI.
Toggle inline value display
Ctrl+M
Displays or hides the values of the variables.
New project
Ctrl+N
Opens
New project
to create a project when no project is opened.
Open project
Ctrl+O
Opens
Open project
to select and open a recently opened project when no project is opened.
Pin/unpin panes
Ctrl+Shift+P
Pins or unpins the selected pane.
Add rung
Ctrl+R
Adds a rung below the selected rung in the LD editor.
Show/hide right panes
Ctrl+Shift+R
Displays or hides the panes that are last pinned to the right of the UI.
Save
Ctrl+S
Saves the controller project.
Save as
Ctrl+Shift+S
Saves a copy of the controller project.
Toggle bit
Ctrl+T
Switches a Boolean variable between on and off states.
Paste
Ctrl+V
Pastes the selected element to the selected position.
New variable
Ctrl+W
Opens
New variable
to create a variable at the current location in the LD, FBD, or ST editor.
Cut
Ctrl+X
Cuts the selected element to the clipboard.
Close pane
Ctrl+Shift+X
Closes the selected pane.
Redo
Ctrl+Y
Redoes the previous command.
Undo
Ctrl+Z
Undoes the previous command.
Show
Connection
Ctrl+Alt+C
  • Displays the
    Connection
    pane if it is hidden.
  • Highlights the
    Connection
    if it is already opened.
Show
Error list
Ctrl+Alt+E
Displays the
Error list
page when the
Output
pane is selected.
Show
Log
Ctrl+Alt+L
Displays the
Log
page when the
Output
pane is selected.
Show/hide
Project Organizer
Ctrl+Alt+P
Displays or hides
Project Organizer
.
Show
Console
Ctrl+Alt+S
Displays the
Console
page when the
Output
pane is selected.
Zoom in
Ctrl++
Zooms in the language editor.
Zoom out
Ctrl+-
Zooms out the language editor.
Previous tab
Ctrl+[
Goes to the previous tab.
Next tab
Ctrl+]
Goes to the next tab.
Close and exit
Ctrl+F4
Closes the controller project and
FactoryTalk Design Workbench
.
Close current tab
Ctrl+Shift+F4
Closes the current tab.
Show tab list
Ctrl+F10
Shows a list of opened tabs to view or close.
Close project
Alt+F4
Closes the current project and returns to the welcome page.
View properties
Alt+Enter
Shows the properties of the selected element in the
Properties
pane.
Highlight
Toolbox
Alt+Insert
Opens and highlights
Toolbox
.
Alt+Insert
has the same effect as
Insert
.
Show/hide FBD grid
Shift+*
Displays or hides the grids in the FBD editor.
Open
Device
menu
Alt+D
Opens the
Device
menu from the menu bar.
Open
Edit
menu
Alt+E
Opens the
Edit
menu from the menu bar.
Open
File
menu
Alt+F
Opens the
File
menu from the menu bar.
Go to rung
Alt+G
Opens
Go to Rung
to enter a rung number to go to.
Open
Help
menu
Alt+H
Opens the
Help
menu from the menu bar.
Open
View
menu
Alt+V
Opens the
View
menu from the menu bar.
Open
Window
menu
Alt+W
Opens the
Window
menu from the menu bar.
Open Help
F1
Opens the context-sensitive Help of
FactoryTalk Design Workbench
.
Edit
F2
Edit the content at the current location.
Delete
Delete
  • Deletes the selected element in the LD or FBD editor.
  • Deletes the selected content or the content to the right of the cursor in the ST editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal