Add a user-defined function block using Project Organizer

Use
Project Organizer
to add a user-defined function block to the controller project.
To add a user-defined function block using Project Organizer
  1. In
    Project Organizer
    , right-click
    User-Defined Function Blocks
    , and then select
    New user-defined function block
    .
  2. In
    New user-defined function block
    , enter the UDFB name, select the UDFB type, and then enter the description as needed.
  3. Select
    Create
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal