Delete a Program Organization Unit

Deleting a Program Organization Unit (POU) removes the POU from
Project Organizer
. Its local variables are also deleted.
Prerequisites
  • The POU is offline.
To delete a POU
  • Do one of the following:
    • In
      Project Organizer
      , right-click the POU, and then select
      Delete
      .
    • In
      Project Organizer
      , select the POU, and then from the
      Edit
      menu, select
      Delete
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal