Add a program to a project

Use
Project Organizer
to add a structured text (ST), ladder diagram (LD), or function block diagram (FBD) program to a controller project.
Prerequisites
  • The controller is offline.
To add a program to a project
  1. In
    Project Organizer
    , right-click
    Programs
    , and then select
    New program
    .
  2. In
    New program
    , enter the program name, select the program type, and then enter the description as needed.
    TIP: The program name must be 1 to 128 characters long, starting with a letter or underscore, followed by letters, numbers, or underscores. The program name cannot contain consecutive underscores.
  3. Select
    Create
    .
    TIP:
    To rename a program, in
    Project Organizer
    , select the program, and then in the
    Name
    box of the
    Properties
    pane, enter the new name. Renaming a user program automatically updates all references to the program.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal