Add a user-defined function using Project Organizer

Use
Project Organizer
to add a user-defined function (UDF) to the controller project.
To add a UDF using Project Organizer
  1. In
    Project Organizer
    , expand
    Assets
    .
  2. Right-click
    User-Defined Functions
    , and then select
    New user-defined function
    .
  3. In
    New user-defined function
    , enter the UDF name, select the UDF type, and then enter the description as needed.
  4. Select
    Create
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal