Rename a user-defined function

Use
Project Organizer
to rename a user-defined function (UDF). Renaming a UDF automatically updates all references to the UDF.
To rename a UDF
  1. In
    Project Organizer
    , go to
    Assets
    User-Defined Functions
    .
  2. Expand
    User-Defined Functions
    , and then do one of the following:
    • Select the UDF you want to rename.
    • Right-click the UDF you want to rename, and then select
      Rename
      .
  3. In the
    User-defined function
    box of the
    Properties
    pane, enter the new name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal