Managing Templates
To access the System Template Editor
In the System Configuration Tool, from the Template menu, click
Manage Templates
.Before adding I/O modules to the system, configure the templates to be used for the required modules. Templates contain segments of configuration. Add, delete, modify, duplicate, archive, and restore templates from the
System Template Editor
. Each template performs a specific function and can only be assigned to one module type. A specific template can be used by multiple modules of the assigned type.Task | Procedure |
|---|---|
Add a template |
|
Modify a template |
|
Duplicate a template |
|
Delete a template |
|
Alphabetically sort the templates |
|
Archive a template | Archiving a template ensures that an entire SYSTEM.INI configuration and associated templates are backed up correctly and available to transfer to another Workstation. Note that from release 3.5, templates are extracted from the SYSTEM.INI file itself, and so only the SYSTEM.INI file needs to be archived. However, if the configuration needs to be transferred to a toolset issue before release 3.5, then a template archive is necessary.
|
Restore a template |
|
Create these types of templates with the
System Template Editor
:Template | Modules | Description |
|---|---|---|
Threshold template | 8402, 8403, 8423, 8424, 8431, 8432, 8433, 8448, 8449 | Defines the state of selected I/O module channels that depend on the input signal to the channel. |
LED template | 8403, 8423, 8424, 8431, 8433, 8442, 8444, 8448, 8449, 8451, 8461, 8471, 8472, 8473, 8480 | Defines the color and mode (flashing, steady, or off) of the channel LEDs for the different channel states. Possible values are Off, Red, Green, Red Flash, or Green Flash. |
Force template | 8402, 8403, 8423, 8424, 8431, 8432, 8433, 8444, 8448, 8449, 8451, 8461, 8471, 8472, 8473, 8480 | Defines the state the unconnected channels must be forced into to provide a healthy (unalarmed) system state. |
System template | 8402, 8403, 8423, 8424, 8431, 8432, 8433, 8442, 8444, 8448, 8449, 8451, 8461, 8471, 8472, 8473, 8480, All Module Types | Defines the timeout intervals for the Watchdog and IMB (Inter-Modular-Bus) of the I/O module. |
Flags template | 8402, 8403, 8423, 8424, 8431, 8432, 8433, 8442, 8444, 8448, 8449, 8451, 8461, 8471, 8472, 8473, 8480 | Defines the flag settings for the I/O module. |
Filter template | 8402, 8403, 8423, 8424, 8431, 8432, 8433 | Defines the internal filtering values for the I/O module. |
Additional CLI | 8402, 8403, 8423, 8424, 8431, 8432, 8433, 8442, 8444, 8448, 8449, 8451, 8461, 8471, 8472, 8473, 8480, All Module Types | Defines additional CLI (Command Line Interface) entries that are external to the configuration data. |
Speed Monitor template | 8442 | Defines the operating parameters required by the speed monitor. |
Shutdown template | 8444, 8448, 8449, 8451, 8461, 8471, 8472, 8473, 8480 | Defines the output action required when the module enters the shutdown state. |
Channel Type template | 8448 | Defines the direction (input or output) for the channels of the module. |
De-energized Short Circuit template | 8448, 8449, 8451, 8461, 8471, 8472, 8473 | Enables short circuit detection for de-energized outputs. |
TIP:
Templates created with the
All Module Types
are
not restricted to a specific module type; apply the template to any I/O module.From the
System Template Editor
, view the list of existing templates. The Quick View pane displays the details of an existing template. 
Provide Feedback