System Templates
The System template enables configuring the following information:
- No-Load Threshold
- Inter-Modular Bus Timeout
- Watchdog Timeout
- Power Fail Timeout
- Bypass Timeout
To configure the System Template
- From theTemplate Creationdialog box, enter the template name, select an applicableModule Type, then select theSystem Template Type, and then clickEdit Template.
TheModuledialog box displays. - In theModuledialog box, do the following:
- To add anIMB Timeout, enter the required value in milliseconds, and then selectAdd.
- To add aWatchdog Timeout, enter the required value in milliseconds, and then selectAdd.
- To add a no-load threshold, in theMiscellaneoussection, enter the required value by using the following syntax:nlthresh = < group1 >, < group2 >,< group3 >,< group4 > [,< group5 >]
- To add a Power Fail timeout, in theMiscellaneoussection, enter the required value by using the following syntax:PWRFAILTO = < value >
- To add a Bypass timeout, in theMiscellaneoussection, enter the required value by using the following syntax:BYPASSTO = < value >
- To complete the configuration, clickOK.
Provide Feedback