Bypass Timeout
The BYPASSTO (Bypass Timeout) is used internally in the module to
bypass the other timeouts during an Active/Standby changeover. The following syntax is used
for the Bypass Timeout:
BYPASSTO = < value >
Only in exceptional
cases will you need to adjust this setting. The timeout value is entered in milliseconds,
and a value of zero disables the timeout.
TIP:
This
value MUST NOT be set to zero for operational systems.
Provide Feedback