De-energized Short Circuit Templates
By default, output modules do not detect for short circuit faults when de-energized. Using the De-energized Short Circuit template, configure output modules to detect de-energized short circuit faults on some or all channels. The impedance below which a de-energized short circuit fault is reported is 40 ohms. The cold resistance of small incandescent lamps may be less than this threshold.
TIP:
De-energized Short Circuit templates will not work on
older 5V HIU hardware builds. An attempt to swap from a 3.3V module with this template, to a
5V module, will fail.
To configure the De-energized Short Circuit Template
- From theTemplate Creationdialog box, enter the template name, select an applicableModule Type, then select theDe-energised Short Circuit Template Type, and then clickEdit Template.
TheDe-energised Short Circuit Detectionwindow is displayed. - In theDe-energised Short Circuit Detectionwindow, do the following:
- To modify the channel line monitoring, right-click the required channel, and then clickOffor40.Also select all channels to set the same value for all channels.
- To set the same value for all channels, clickSelect All, right-click in the channel list, and then clickOffor40.
- Configure all required channels and then clickOK.
Provide Feedback