Shutdown Templates
The shutdown template enables configuring individual shutdown states
for each channel of an output module. Output channels are driven to the default fail-safe
state when the module enters the shutdown mode. Typically the module enters the shutdown
mode when any of the system timeouts occur, or when commanded by the TMR Processor. A
channel can be configured to enter a specific shutdown state other than the default using
the Shutdown template.
A shutdown entry is entered using the following
syntax:
channel#=< ON | OFF | HOLD >
The available shutdown
modes are:
Mode | Description |
|---|---|
ON | Energize the output |
OFF | De-energize the output |
HOLD | Hold, or maintain the output in the last commanded state |
All output channels used for safety critical applications must be configured with a
shutdown mode that places the process in the safe state.
To
configure the Shutdown Template
- From theTemplate Creationdialog box, enter the template name, select an applicableModule Type, then select theShutdown Template Type, and then clickEdit Template.
TheShutdown Editordisplays. - In theShutdown Editor, to define the default shutdown value, right-clickDefaultin the list of channels, and then click one of the following:
- On
- Off
- Hold
- UnconfiguredThe default shutdown value is defined.
- In theShutdown Editor, to define the shutdown value for a channel, right-click the required channel and then click one of the following:
- On
- Off
- Hold
- Unconfigured
- Default
- Configure all required channels and then clickOK.
Provide Feedback