Additional CLI Templates
Configure additional CLI templates as required.
To configure an Additional CLI template
- From theTemplate Creationdialog box, enter the template name, select an applicableModule Type, then select theAdditional CLI Type, and then clickEdit Template.
TheCLI Entrydialog box displays. - In the CLI Entry dialog box, do the following:
- To add an instruction, in thePlease Enter CLI Instructiontext box, type the required operation syntax, and then clickAdd Entry.
- To delete an instruction, in theCurrent CLI Entrieslist, select the entry to remove and then clickRemove Entry.
- To complete the Additional CLI template configuration, clickOK.
Provide Feedback