LED Templates
LED templates define the mapping between the front panel indicators for the specific module and the input or output state. LED templates are available for the following:
- Input Modules
- Output Modules
- Zone Interface Modules
Provide Feedback