LED Templates for Input Modules
The LED template defines the mapping between the input state and the front panel indicators for the specific module. Use the LED State Editor to map the required operation for all input channels. An LED mapping entry is made using the following syntax:
state# = <OFF | RED | GREEN [+FLASH]>
If no entries are made in this section, the module will operate with the default LED mapping. The following example displays the default values for the 8403 Digital Input Module, which are suitable for inputs without line monitoring devices installed.
State for Input Modules | State for 8449 Module | Default Value | Description |
|---|---|---|---|
0 | 8 | = Red | Out of range |
1 | 9 | = Off | Open circuit |
2 | 10 | = Off | Open field contact |
3 | 11 | = Off | Indeterminate contact state |
4 | 12 | = Green | Closed field contact |
5 | 13 | = Green | Short circuit |
6 | 14 | = Green | Over range |
7 | 15 | = Off | |
8 | - | = Red |
TIP:
State 7 represents a module fault. States 8 through 15
all represent channel fault states (except for the 8449 Valve Monitor module). For the 8449
module, states 8 through 15 are used differently since the valve outputs and position inputs
are grouped in pairs.
LED templates define specific LED states. For example, if inputs are installed with line monitoring devices, the LED mapping entries can be made to flash red for the corresponding states that indicate a line fault condition, such as Open circuit, Indeterminate and Short circuit.
To configure the color and operating modes of the LED front panel indicators
- From theTemplate Creationdialog box, enter the template name, select an applicableModule Type, then select theLED Template Type, and then clickEdit Template.
TheLED State Editordisplays. - To modify the color and operating mode of the channel, click the required state LED icon, and then click one of these:
- Off
- Red
- Green
- Red Flash
- Green FlashThe modified channel LED of the input module displays.
- In theLED State Editor, configure the required input channel states, and then clickOK.
Provide Feedback