LED Templates for Zone Interface Modules
Trusted®
8448 Zone Interface Modules can have each channel defined as an input or an output using the Channel Type Templates. The LED State Editor
enables configuring individual channels with an LED state/color map.When configuring the channels, apply the defined default values for the channel or set different values. Channels using the default LED mapped state are identified with
.
. Task | Procedure |
|---|---|
Configure the LED states for the channels of the 8448 Zone Interface module |
|
Assign a specific channel mapping as the default mapping |
|
Assign the default mapping states to a channel retained as specific |
|
Provide Feedback