Speed Monitor Templates
To use the T8442 TMR Speed monitor module, configure the Speed Monitor template.
TIP:
For information on the Speed Monitor template, refer to
the
Trusted®
T8442 TMR Speed Monitor product description.To display the Speed Monitor Configuration
- From theTemplate Creationdialog box, enter the template name, select the 8442 Module Type, then select theSpeed Monitor template Type, and then clickEdit Template.

Provide Feedback