Force Templates
The Force template enables forcing the input or output channel states on-board the module to a specific value irrespective the current value. Channels may be forced to a specified state on a per-channel basis. The states that exist on a module are specific to that module. Use the
Forcing Editor
to add, remove, or modify Force templates.
ATTENTION:
Refer to the Safety Manual.
Example: channels on the 8431 Analog Input Module can be in any one of the following states:
State | Description |
|---|---|
0 | Under range |
1 | Low-low |
2 | Low |
3 | Normal |
4 | High |
5 | High-high |
6 | Over range |
7 | Fail safe |

In this example, channels 1, 11, and 22 are forced to the High state (4).
To configure the Force Template
- From theTemplate Creationdialog box, enter the template name, select an applicableModule Type, then select theForce Template Type, and then clickEdit Template.TheForcing Editordisplays.
- To add a channel force to the template, select the required channel number in theChannel Selectwindow, then enter the required channel state in theChannel Statewindow, and then clickAdd.
- To remove a channel from the template, select the channel, and then clickRemove. A warning message confirms the removal of the correct force.
- To modify the state of a channel, select the required channel, then enter the new value in theChannel Statewindow, and then clickChange.
- Configure all required channels, and then clickOK.
Provide Feedback