Working in the Development Environment

In the development environment, perform many tasks:
  • View output messages in the
    Output
    window
  • View build errors in the
    Error
    List
  • Zoom the contents of program organization units (POUs)
  • Arrange and dock windows
  • Perform searches of the development environment from different windows
  • Navigate the development environment with the
    Windows
    dialog box
  • Customize, create, and rename toolbars and commands
  • Export, import, or reset environment settings with the
    Import
    and
    Export
    Settings
    Wizard
  • Use keyboard shortcut combinations to perform multiple actions
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal