Customize Toolbars

For standard toolbars, modify docking locations. For custom toolbars, modify docking locations, rename toolbars, and delete toolbars. The
Customize
dialog box lists the provided toolbars and any custom user toolbars.
To customize a toolbar
  1. From the
    Tools
    menu, click
    Customize
    ...
  2. From the
    Customize
    dialog box, click the
    Toolbars
    tab, make the required changes, and then click
    Close
    .
    • To modify the docking location for a toolbar, select the required toolbar from the
      Toolbars
      list, click
      Modify
      Selection
      , then click the preferred location for docking the toolbar. Available docking locations are top, left, right, and bottom.
    • To rename a custom toolbar, select the required toolbar from the
      Toolbars
      list, click
      Modify
      Selection
      , and then type the required name in the text field.
    • To delete a custom toolbar, select the required toolbar from the
      Toolbars
      list, and then click
      Delete
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal