Customize Commands
Customize menu bar, toolbar, and contextual menu commands by selecting a set of commands, then choosing an individual command to modify using the available options. Add, rename, reset, delete, and rearrange the order of commands in the menus. Also delimit groups of commands in menus and specify display options.
Customize different levels and options for menu items including categories and subcategories.
Perform these menu tasks:
Task | Procedure |
|---|---|
Add a menu category to the menu bar |
|
Add a menu item to an existing menu category, toolbar, or contextual menu | Menu items are either commands or subcategories leading to submenus. Before adding a menu item, arrange the required order by selecting the menu item following the location of the new item in the list or rearranging the menu items after insertion.
|
Reset menu bars, toolbars, or contextual menus | To reset all environment settings to the default, select Tools > Import and Export Settings and then Reset All .
|
Delete a menu item, toolbar, or contextual menu |
|
Create a group of commands | Create groups of commands by inserting separator bars.
|
Rearrange menu items |
|
Provide Feedback