Create Toolbars
Create custom toolbars to use in the development environment.
To create a custom toolbar
- From theToolsmenu, clickCustomize...
- From theCustomizedialog box, click theToolbarstab, and then clickNew.
- In theNewToolbar dialog box, type a name for the custom toolbar, and then clickOK.The custom toolbar name adds to theToolbarslist.
Provide Feedback