Specify the command display options

Initially, the display options for commands are set to default. In menus, the default display option is
Image
and
Text
, while in toolbars it is
Text
Only
(in Menus)
. The
Text
Only
(in
Menus)
option displays an image in a toolbar or text in a menu. The
Text
Only
(Always)
option displays text in a menu or toolbar. The
Image
and
Text
option displays both image and text in a menu or toolbar. Do not associate an image with a command.
To specify the display options for a command
  1. From the
    Tools
    menu, click
    Customize
    ...
  2. From the
    Customize
    dialog box, click the
    Commands
    tab
  3. Select the menu to modify from the
    Menu
    bar
    ,
    Toolbar
    , or
    Context
    menu
    drop-down combo boxes.
  4. To specify the display options, select the required command in the
    Controls
    list, click
    Modify
    Selection
    , then click one of these:
    • Default
      style
    • Text
      Only
      (Always)
    • Text
      Only
      (in Menus)
    • Image
      and
      Text
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal