Zooming the Contents of Active POUs
Set the zoom factor for viewing the contents of individual active graphic program organization unit (POU) documents:
- Zoom in, enlarges the contents of an active graphic POU document
- Zoom out, provides a larger overview of the contents of an active graphic POU document, as if viewed from further away
- Zoom to fit all, sets the magnification factor to display the contents within the width and height of an active graphic POU document
- Zoom to page width, sets the magnification factor to display the contents within the width of an active graphic POU document
- Zoom percentage factor, enables specifying the magnification factor for the contents of an active graphic POU document
To set the zoom factor for an active POU document
- Click the active graphic POU document for which to adjust the zoom factor.
- From theZoomtoolbar, click the required zoom option.
Provide Feedback