Displaying the Output Window
To access the Output window
From the View menu, click
Output
(or press Ctrl+Alt+O
).Review generated messages from the
Output
window. From the Output
window, perform these tasks:Task | Procedure |
|---|---|
Review generated status messages |
|
Manage the contents of the Output window | Manage the word wrapping and clear the contents of the window.
|
Output
window toolbar commands are:Show output from: | Selects individual features for which to view generated status messages |
|---|---|
Find Message in Code | Moves the insertion point to the line in the language editor containing the selected build error |
Go to Previous Message | In the Output window, jumps to the previous build error message. In the code editor, locates the build error and automatically moves the insertion point to the error. |
Go to Next Message | In the Output window, jumps to the next build error message. In the code editor, locates the build error and automatically moves the insertion point to the error. |
Clear all | In the Output window, deletes all displayed messages. |
Toggle Word Wrap | Wraps text to continue on the next line for messages extending beyond the viewing area |
Provide Feedback
.
.
Find Message in Code
Go to Previous Message
Go to Next Message
Clear all
Toggle Word Wrap