Use the Error List
Use the
Error
List
to view errors, warnings, and messages produced when editing program organization units (POUs) and performing build operations.Navigate from one error to the next using the contextual menu options. Also navigate between errors using the keyboard arrows.
Column | Description |
|---|---|
Category | Displays an icon identifying the type of error |
Default Order | Displays an integer indicating the order in which the error occurred relative to the other errors |
Description | Displays the error message text |
File | Displays the POU name or the POU location and POU name |
Line | Displays the line number |
Column | Displays the column number |
Project | Displays the name of the project |
Error List toolbar commands are:
Icon | Description |
|---|---|
![]() | Displays the number of generated errors. Click to toggle between displaying and hiding the errors in the list. |
![]() | Displays the number of generated warnings. Click to toggle between displaying and hiding the warnings in the list. |
![]() | Displays the number of generated messages. Click to toggle between displaying and hiding the messages in the list. |
Sort the contents of the
Error
List
. Customize the Error
List
by resizing columns and arranging the columns to display.Task | Procedure |
|---|---|
Display the Error List |
|
Sort errors |
|
Search messages in the Error List |
|
Customize the Error List |
|
Provide Feedback