Navigating in the Development Environment

Navigating in the development environment is simplified with the use of the
Windows
dialog box. The
Windows
dialog box displays the active files open in the current project. Active files consist of language containers, the
Application View
and other windows docked in the workspace.
wde_nvw
From the
Windows
dialog box, perform these tasks for active files:
  • Switch between active files
  • Save changes to one or more active files
  • Close active files
To navigate using the Windows dialog box
  1. From the
    Window
    menu, click
    Windows
    .
    The
    Windows
    dialog box displays the list of active files.
  2. To switch to another active file in the list, select the required file, then click
    Activate
    .
  3. To save changes to active files, select the required files from the list, then click
    Save
    .
  4. To close active files, select the required files from the list, then click
    Close
    Window(s)
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal