Importing and Exporting Settings

Import or export specific categories of settings, or reset the environment to one of the default collections of settings. The environment settings include the settings for the various development views, editors, and tools.
  • Export Selected Environment Settings
  • Import Selected Environment Settings
  • Reset all Settings
To import, export, or reset environment settings
  1. From the
    Tools
    menu, click
    Import
    and
    Export
    Settings.
  2. Select the required option, then follow the on-screen instructions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal